This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: Using TIDEP-01012 for close-medium range imaging

Part Number: TIDEP-01012

Is there any showstopper in using the cascade setup for imaging breathing patterns at close/medium range? Is it even possible? If so, I realize you have not tried it but can you provide any advice on attempting this? Thanks

  • Hi

    Can you please provide more details about "imaging breathing pattern"?

    Why do you think that a cascade setup is needed vs a single sensor solution?

    thank you

    Cesar

  • Hi Cesar,

    Thank you for the reply and I apologize for the lack of clarity.

    By “imaging breathing patterns”, I mean acquiring a 2D image (point cloud) of a person with some information of the displacements of the chest at each point. The standard sensors from my understanding require a very good alignment of the antenna with the chest of the person. The demos for breathing monitoring show only one reading of the overall chest displacement. Would a phased array not provide better capability to detect  displacements at various angles, therefore make it possible to create a 2D map?

    Hope that clarifies the question.

    Thanks

  • Hi,

    We don't have any experience with such applications.

    You would need to perform testing

    thank you

    cesar