Other Parts Discussed in Thread: UNIFLASH,
Hi,
My customer is trying to create their custom board using AWR1243P(s) and they have some questions about pin handing.
1. They can't find SOP pins on AWR1243P datasheet. Which pins are corresponding to SOP[2:0] ? Also, the pin state for flashing mode (via uniflash) and normal operating mode is not mentioned when releasing the reset.
2. Is it okay to open P1/P2/P3/R2/C13/C14 pins as the datasheet suggests in Figure 7-3 AWR1243 Reference Schematic? Not exactly sure about the purpose of these pins.
3. I believe JTAG related pins can be floating because these are only ti internal use. Correct ?
Best Regards,
NK