This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP432: Data hold time in 100kHz frequency

Part Number: TMP432

Hello E2E,

We have a question on data hold on time.

In fast mode, the data hold time range is from 20ns as min to 900ns as max.

In customer application, they use 100kHz clock frequency as normal mode on i2c interface and the data hold on time is longer than 5us.

Is that ok?

we are confused a little bit.

according to the figure 13 i posted below, the data hold time should be larger than ON time of clock.

In fast mode, the clock frequency is 400kHz and ON time of clock is 1.25us, but the maximum data hold time is 900ns.

please help to clarify our question.

BR,

Jason