This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Multi Channel Mode

Guru 29720 points
Part Number: OPT3101


Hi Team,

I would like to aks the following questions.

1)
Could you tell me the situation Multi Channel Mode is used?
Is there any application note?

2)
Is it possible to activate three channels (TX0, TX1, TX2) simultaneously?
I believe it isn't possible however would like to confirm just in case.
My customer wants to increase illumination driver current more than 173mA.

Best Regards,
Yaita