Part Number: LDC2112
Regarding the circuit, I have some questions: as following.
Please take a look and advise after your return.
thanks.
1.LDC2112 SCL/SDA can be 3.3V level, but other IO pin only can be 1.8V level right?
2. Is this inductance value from the calculation form?
3. I use IN0 only, can I choose either OUT0 or INT to connect to the MCU for interrupts?