This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Is there any suggestion on how to test the velocity and velocity resolution?

Part Number: AWR1843

Hi,

 As title, is there any suggestion on how to test the radar target velocity and velocity resolution?

 If I have one ARTS simulator, how can I leverage such tool for it?

  • Hello Jesse,

    If this is a radar object simulator then you can use it with AWR1843 device. To test the velocity, you need to simulate an object with a specific velocity and set the required configuration to the device (using mmWave Studio). Capture and process the data to check the velocity accuracy.

    To test velocity resolution you need to simulate two different objects (same range) with a small velocity difference and repeat the above experiment.

    Regards,

    Jitendra

  • Hi Jitendra,

     My customer has the ARTS simulator can be used for the test. I will check with them if the ARTS can simulate 2 moving objects.