This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPIO-4: maximum number of LMP91000EVM boards that can be connected?

Part Number: SPIO-4
Other Parts Discussed in Thread: LMP91000EVM, LMP91000

Hello!

LMP91000EVM user guide says that it connects to the SPIO4 board through the SPIO-GPSI16 connector. There is only 1 header for this and it seems that only one LMP91000EVM can be connected to SPIO4.

However, I was wondering if it's possible to have 2 LMP91000EVMs connected to SPIO4 because the SPIO-4 user guide mentions in section 2.5 that the upper portion can be used if bidirectional signals are required by the DUT.

Hoping for your advice.

Thank you!