Other Parts Discussed in Thread: LDC1614, , LDC1314
Hi,
we are building a new instrument for array testing. Each system uses 32 of the LDC1614 (one for each channel). In order to test if the LDC1614 provides good performance we bought a Eval Board (LDC1614EVM) but so far we could not get it to work correctly.
Main issue: the value displayed by the EVM PC software (TI's Sensing Solution GUI) only varies few hundred points instead of the full 12 bit range. We tried following the instruction of the datasheet but maybe done something incorrectly.
Goal: to have the output (on the TI's Sensing Solution PC software) to swing full 12-bit scale with out inductor's value ranging from 79 to 81 uH
Can you please:
- outline the detailed configuration of the guy and the EVM
- the capacitor value to use in parallel with the inductor
- how to set the frequency ideally to 200KHz
Here are the full details of the coil and of the applicaiton/system:
- coil details: 8mm ID diameter - 79 turns of 0.8m wire - 82 uH inductance (at rest) - 7.9 ohms
- the inductance variation we are trying to measure varies from 79 to 81 uH
- ideal working frequency 200KHz
- capacitor value: please advise
Because of the urgency and tight timescales, in order to avoid going back and forth with additional questions could I ask you to please outline all the calculations/procedures. Please not just a cut and paste from the datasheet because we already tried all described in there and clearly could not get it to perform correctly.
Many thanks
Riccardo