Part Number: AWR1642BOOST-ODS
Hello,
Project : Obstacle detection lab from ti automotive toolbox(2.7.1)
Device : awr1642boost-ods
The ods_3d_visualizer.exe works well when guiMonitor is set to default value (1 1 0 0 ) in config file.
When I set guiMonitor to (1 1 1 0) , I see the points, clusters and azimuth heatmap for first 25 seconds. The screen freezes for the next 10 seconds. After that , I see all the outputs again and the freezing/unfreezing cycle repeats.
Any reason why this might be happening ?
Thank you,
Pranav.