This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST:Flashing through UART without the XDS110(TM4C129)

Part Number: IWR1443BOOST

Hi,aozer

I saw your response in another thread:

e2e.ti.com/.../822063

you suggest that You can also just use a USB to FTDI cable instead of the XDS110 debug probe.https://www.alliedelec.com/product/ftdi/ttl-232r-rpi/70403954/?gclid=EAIaIQobChMI-pXD05fv4wIVYP_jBx0rBQ7vEAQYAyABEgIE2fD_BwE&gclsrc=aw.ds

If we use FTDI TTL-232R-RPI adapter cable, do we need to use two? The reason is that I saw in some threads that flashing needs to connect the four wires AR_RS232TX, AR_RS232RX, AR_MSS_LOGGER, and GND, but one FTDI TTL-232R-RPI transfer line can only provide RX, TX, and GND. Do we need a second one to connect to AR_MSS_LOGGER?
By the way, can I use the adapter cable of CH340 chip?

Regards,

Javid