Other Parts Discussed in Thread: AWR1243
Hi,
I was working with the 4 cascaded chips; however, it is very confusing for me that what is the numbering of the devices in lua commands? What is the binary file associated with each device?
Just to mention, I read all the cascade docs including "AWR1243 Cascaded Radar RF Evaluation Module" and "mmwave_studio_cascade_user_guide". In the former, the devices are numbered in figure 2 of page 6 but in referring the master, slave1, slave2, slave3 in lua commands they are 1,2,4,8. Am I right? I think to get my answer, it is better to give me an example of chirp configurations by lua commands such that I will use "RX Array A" in figure 13 of "AWR1243 Cascaded Radar RF Evaluation Module" when only 5 Tx antennas will become active in a proper sequence such that it makes a virtual MIMO array of 40 antennas. To do that, every other of the Tx azimuth antennas should be activated. Then, I need to know which binary files are associated with the two right chips on the board.
Best,
Mostafa