This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: AWR1243 Capture + Radar Object Detect (DSP) (MIMO) + Null in Cascade Radar Usecases

Part Number: AWR1243
Other Parts Discussed in Thread: MMWCAS-DSP-EVM, MMWCAS-RF-EVM

Hi Team,

The customer is experiencing below issue and needs your help.

He followed the steps of the Processor SDK – Radar (v03.07) User Guide to set the SD card as the boot disk and booted--> Selected the use case and TFDTP--> run matlab--> Got the above error (Can display interface).  Running the GUI control is 1 1 0 0 1 but no data is received. Is the IP address not set correctly? Host IP is 192.168.20.33.

Thanks.

Annie