This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: How to implement coherent integration in AWR1243 device?

Part Number: AWR1243
Other Parts Discussed in Thread: AWR1642

How to implement coherent integration in AWR1243 device?

Vivek mentioned the following message.

"Hello ,

Lets take an example. The thermal noise is -174dBm/Hz . If we take a noise figure of 14dB the noise level on the receiver is -160 dBm/hz.

If you have a 512 samples per chirp and 5Mhz IF bandwidth , the bin size of each FFT bin is 5Mhz/512 = 9.765Khz. So the noise level per FFT bin in a chirp is = -160+10log10(9765) = -120 dBm.

If you do coherent integration across 512 chirps in a frame that gives you a noise reduction of 27 dB (10log512). So across a frame the noise level is -120-27 = -147dbm.

If you set a detection SNR of 15dB then you can detect an object at -122dBm input level.

Regards,

Vivek

"

Thanks in advance.