This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Questions about using the DCA1000's cli tool

Part Number: DCA1000EVM

Hi Team,

Customer sees in the software user's guide of the cli that he can control the DCA1000 through the cli tool and finally achieve the task of data collection. This looks like he can write mmwavestudio-like functions only through the cli tool. He tries using the cli tool, and he can really control DCA1000, but it seems that only DCA1000 can be configured. In mmwavestudio we can also configure the radar board, such as waveform configuration and so on. But he doesn't see related configuration commands in the cli tool. The customer wants to confirm whether it is possible to control the DCA1000 only with the cli tool and the radar EVM board to achieve the collection of raw data? If yes, could you explain how to configure the parameters of the radar waveform?

Thanks.

Annie