This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: [ITB4.2.0 - 3D people counting] When cfg is sent to device while it is already running, it doesn't send back "Done" to "sensorStart".

Part Number: IWR6843ISK-ODS

Hi,

I am running 68xx_3D_people_counting lab in mmwave_industrial_toolbox_4_2_0 using the following FW and cfg.

FW:"C:\ti\mmwave_industrial_toolbox_4_2_0\labs\people_counting\68xx_3D_people_counting\prebuilt_binaries\3D_people_count_68xx_demo.bin"

cfg:"C:\ti\mmwave_industrial_toolbox_4_2_0\labs\people_counting\68xx_3D_people_counting\chirp_configs\ODS_6m_default.cfg"

When I send the cfg file above to the device through serial port just after turning on the device, it returns "Done" to "sensorStart" command and starts sending radar data back to PC.

However, while it is already running, when I send the cfg file to it again, it doesn't return "Done" or even an error, and stops sending radar data.

Why is this so?

Best regards,

Fields