Tool/software: Code Composer Studio
Hello.
We have an issue with the IWR1642BOOST, which we can only start ( the people counting demo) after flashing it but, when we want to stop it (it stops successfully) and start again the problem occurs! When we send start command again (without flashing). We get DONE from the device but it does not starts (flush command does not help). To start it again when we have to remove supply voltage.
This is copied communication (cfg file), after sensorStop command, we send sensorStart command, get DONE, but no data are transmitted...
dfeDataOutputMode 1 dfeDataOutputMode 1 Done mmwDemo:/> mmwDemo:/>channelCfg 15 3 0 channelCfg 15 3 0 Done mmwDemo:/> mmwDemo:/>adcCfg 2 1 adcCfg 2 1 Done mmwDemo:/> mmwDemo:/>adcbufCfg 0 1 1 1 adcbufCfg 0 1 1 1 Done mmwDemo:/> mmwDemo:/>profileCfg 0 77 30 7 62 0 0 60 1 128 2500 0 0 30 profileCfg 0 77 30 7 62 0 0 60 1 128 2500 0 0 30 Done mmwDemo:/> mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 0 0 0 0 0 0 0 1 Done mmwDemo:/> mmwDemo:/>chirpCfg 1 1 0 0 0 0 0 2 chirpCfg 1 1 0 0 0 0 0 2 Done mmwDemo:/> mmwDemo:/>frameCfg 0 1 128 0 100 1 0 frameCfg 0 1 128 0 100 1 0 Done mmwDemo:/> mmwDemo:/>lowPower 0 1 lowPower 0 1 Done mmwDemo:/> mmwDemo:/>guiMonitor 1 1 0 0 guiMonitor 1 1 0 0 Done mmwDemo:/> mmwDemo:/>cfarCfg 6 4 4 4 4 16 16 4 4 50 62 0 cfarCfg 6 4 4 4 4 16 16 4 4 50 62 0 Done mmwDemo:/> mmwDemo:/>doaCfg 600 1875 30 1 doaCfg 600 1875 30 1 Done mmwDemo:/> mmwDemo:/>SceneryParam -6 6 0.05 6 SceneryParam -6 6 0.05 6 Done mmwDemo:/> mmwDemo:/>GatingParam 4 3 2 0 GatingParam 4 3 2 0 Done mmwDemo:/> mmwDemo:/>StateParam 10 5 10 100 5 StateParam 10 5 10 100 5 Done mmwDemo:/> mmwDemo:/>AllocationParam 450 0.01 25 1 2 AllocationParam 450 0.01 25 1 2 Done mmwDemo:/> mmwDemo:/>VariationParam 0.289 0.289 1.0 VariationParam 0.289 0.289 1.0 Done mmwDemo:/> mmwDemo:/>PointCloudEn 1 PointCloudEn 1 Done mmwDemo:/> mmwDemo:/>trackingCfg 1 2 250 20 200 50 90 trackingCfg 1 2 250 20 200 50 90 Done mmwDemo:/> mmwDemo:/>sensorStart sensorStart Done mmwDemo:/> mmwDemo:/>sensorStop sensorStop Done mmwDemo:/> mmwDemo:/>sensorStart sensorStart Done mmwDemo:/>
Thank you.
Lukas