Other Parts Discussed in Thread: MMWAVEICBOOST, , UNIFLASH
I only have IWR6843AOP. Can I do the People Counting experiment?Or must IWR6843AOP be installed on mmwaveicboost?
and What demo experiments can IWR6843AOP do?
Thanks for your help
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I only have IWR6843AOP. Can I do the People Counting experiment?Or must IWR6843AOP be installed on mmwaveicboost?
and What demo experiments can IWR6843AOP do?
Thanks for your help
Hi Akash,
I used Uniflash to download the 3D_people_count_68xx_demo.bin program to IWR6843AOP, and successfully connected to IWR6843AOP using mmWave_People_Counting_GUI.
But after sending configuration, there is no any other output into display area.
So I guess it's because I didn't use MMWAVEICBOOST.
Is my guess right?
Is there any way to only use IWR6843AOP to do People Counting demo?
Thank you
Hi User,
The AOP board is an ES1 device, and the demo only works with ES2 devices. If you want to run on ES1, you can recompile with SDK 3.2.x. You will have to deal with a few errors that come up during compilation as the function calls have changed from SDK 3.2 to 3.3
Regards,
Justin