Other Parts Discussed in Thread: LDC1614
Hi, I am developing a solution to measure the capacitance of a StretchSense soft robotic sensor (SRS) (see: https://stretchsensed.wpengine.com/wp-content/uploads/2019/03/SSD18-Datasheet.pdf). I had a couple questions about the FDC2214 for use in this application.
1: In the FDC2214 datasheet, there is a clause under the "Do's and Don'ts" section that states that hot-swapping sensors should not occur. I would like to retain the ability to connect and disconnect the SRS without powering down the IC (the SRS is connected with standard 0.1" pitch headers). Does this classify as hot-swapping? Are there any workarounds?
2: To ensure we can sense all values of capacitance, I would like the design to be capable of sensing 200pF-2000pF. Is this a reasonable range for the FDC2214? Would properly selecting the LC resonator components enable this range? What resolution would we expect for such a range?
Thanks,
Preston Peranich