Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843, , IWR6843AOP
Can the DCA100EVM be paired with IWR6843 and the MMWAVEICBOOST to capture RAW I/Q data real time?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the DCA100EVM be paired with IWR6843 and the MMWAVEICBOOST to capture RAW I/Q data real time?
The data capture through radar studio is real time capture. But the captured data is saved as a binary file at the end of the capture. And the process can be applied at the end of the capture. We do not support real time process during capture.
Best,
Zigang
So can the iwr6943AOP, dca1000evm, and the mmwaiceicboost be used all together at once to capture data?
The radar studio based data capture is using DCA1000 + mmwaveICBoost + EVM board. IWR6843AOP is supported too.
Best,
Zigang