This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: TX antennas used in object detection usecase

Part Number: MMWCAS-DSP-EVM

Hi,

I am working on the object detection usecase.

In the PROCESSOR SDK Radar Datasheet I read that this usecase is runned using 8 Tx Antennas (pag17) and in the source code it is defined 

/* Total number of Txs across sensors that are chirped as part of TDM-MIMO */
#define CHAINS_CASCADE_RADAR_NUM_TX_ANTENNA (8U) 

But reading the code for sensors configuration I see that there are 10 chirps in each frame, and I understand that the number of TX antennas used in total is 10, 3 for master and two of the slaves and only one for the last slave. 

Is there an error in the datasheet and in "CHAINS_CASCADE_RADAR_NUM_TX_ANTENNA"  definition or am I misunderstanding ?

Thank you, 

Sara Salvador