Other Parts Discussed in Thread: IWR1642, DCA1000EVM
hello,
I'm using the iwr1642+mmwave devpack to read adc data from the radar.
i've realized from the forums and the user's guides that an additional to the devpack ,tsw1400evm is required, or instead-the entire setup could be replaced with a dca1000evm.
which benefits do i get from each approach? (adding another cards/replacing the entire thing)
which one of them is recommended?
all the best,
Oren