This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/IWR1443: Use IAR Compiler and HAL Code Generator with IWR1443

Part Number: IWR1443


Tool/software: TI C/C++ Compiler

Hi,

We are currently using the Texas ARM Compiler version 16.9.6.LTS to build the MSS firmware, but since IAR is our preferred compiler for ARM cores, we would like to test building the MSS code with an IAR compiler. We use the HAL Code Generator to set up the project. Unfortunately, IWR1443 is not amoung the selectable devices. My question is therefore: Which of the following devices will best match the IWR1443 MSS core?
BR,
Hakan