Other Parts Discussed in Thread: IWR6843,
Hello,
I got the below questions from a customer.
1.) TI 3D People counting demo firmware for IWR6843 is using Capon beamforming for point detection. Wonder why other TI firmware which return point clouds only does not use capon beamforming ? Is there any plan to add capon beamforming for normal point cloud firmware. Our understanding is that capon beamforming is more accuracy for point detection.
2.) The TI 3D people counting demo firmware seems to be designed for wall mount antenna. Does it support the IWR6843ISK-ODS ? Seems we can change antGeometry0/antGeometry1 for ODS antenna, anything we need to change to support that ?
3.) In order to cover a larger space for people counting, we might want to use two or more IWR6843 sensors, but we need full 4G bandwidth for full precision. So cannot do frequency division multiplex between devices. Since there are overlapped region between sensors to ensure coverage, what is the best way to avoid interference ?
4.) Does TI have some kind of detection when interference occurs ?