This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: LDC1101

Part Number: LDC1101

If a sensor coil is moving with 3m/sec linearly. Can it detect any defect in metal? 

please suggest.

  • Shivam,

    That is not a suggested application for TI's inductive sensing portfolio. Here are the reasons why I don't think it will work:

    - An Rp measurement could help detect a compositional change in the metal, but Rp measurements are best suited for identifying several distinct metals. It may not do well identifying small changes.

    - Rp varies quite a bit with temperature, which is one of the reasons why it is unsuitable for detecting small changes.

    - L measurements are good for detecting changes in distance, but it would not be able to detect small spurs or defects that are much smaller than the coil size.

    - Any changes in distance from the metal to the coil as the coil is moved will change the Rp and L readings. So you will be unable to tell if the delta is due to a defect or due to a small distance change

    - tilt of the metal or coil will also look like a distance change