Part Number: LDC1000
Hi,
I've recently inherited a design based on the LDC1000. Two queries.
Readings of the proximity data registers are highly sensitive to temperature. I understand this is due to the inherent temp co of our PCB based sensor winding.
As the temperature rises the LDC1000 responds in steps. Say I heat the equipment from 25degC to 30degC the proximity data increases roughly linearly with temperature, as I continue to heat it to 38degC the proximity data is stuck at 4764, then it rises linearly for a while then it gets stuck at 4992. Is this due to the LDC1000's operation ? The data sheet and the various application notes don't explain how precisely the external circuit is excited or measured by the LDC1000.
Secondly, we use LDC1000 TSSOP16 to measure RP (rather than inductance), it is going obsolete. Is there a drop in replacement ?
Regards
Richard