Hello
i using ldc1101 with stm32h7 MCU. I am using 12 Mhz external oscillator at CLKIN pin and coil which is come with LDC1101 EVM.
After setting these values on register
LDC1101_WRITE(_LDC1101_REG_CFG_RP_MEASUREMENT_DYNAMIC_RANGE,0x07);
// LDC1101_WRITE(_LDC1101_REG_CFG_INTERNAL_TIME_CONSTANT_1,0x90);
// LDC1101_WRITE(_LDC1101_REG_CFG_INTERNAL_TIME_CONSTANT_2,0xA0);
// LDC1101_WRITE(_LDC1101_REG_CFG_RP_L_CONVERSION_INTERVAL,0x03);
// LDC1101_WRITE(_LDC1101_REG_CFG_ADDITIONAL_DEVICE,0x00); // 0x01
// LDC1101_WRITE(_LDC1101_REG_RP_THRESH_H_MSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_RP_THRESH_L_LSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_RP_THRESH_L_MSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_CFG_INTB_MODE,0x00);
// LDC1101_WRITE(_LDC1101_REG_CFG_POWER_STATE,_LDC1101_FUNC_MODE_SLEEP_MODE);
// LDC1101_WRITE(_LDC1101_REG_AMPLITUDE_CONTROL_REQUIREMENT,0x00); // 0x01
// LDC1101_WRITE(_LDC1101_REG_L_THRESH_HI_LSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_L_THRESH_HI_MSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_L_THRESH_LO_LSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_L_THRESH_LO_MSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_LHR_RCOUNT_LSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_LHR_RCOUNT_MSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_LHR_OFFSET_LSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_LHR_OFFSET_MSB,0x00);
// LDC1101_WRITE(_LDC1101_REG_CFG_LHR,0x00);
//LDC1101_WRITE(_LDC1101_REG_CFG_RP_MEASUREMENT_DYNAMIC_RANGE,_LDC1101_RP_SET_RP_MAX_24KOhm | _LDC1101_RP_SET_RP_MIN_1_5KOhm);
// LDC1101_WRITE(_LDC1101_REG_CFG_INTERNAL_TIME_CONSTANT_1,_LDC1101_TC1_C1_0_75pF | _LDC1101_TC1_R1_21_1kOhm);
// LDC1101_WRITE(_LDC1101_REG_CFG_INTERNAL_TIME_CONSTANT_2,_LDC1101_TC2_C2_3pF | _LDC1101_TC2_R2_30_5kOhm);
// LDC1101_WRITE(_LDC1101_REG_CFG_RP_L_CONVERSION_INTERVAL, 0xD0 | _LDC1101_DIG_CFG_RESP_TIME_768s);
// LDC1101_SetPowrMode( _LDC1101_FUNC_MODE_ACTIVE_CONVERSION_MODE);
// LDC1101_goTo_LHRmode(Prox1);
after setting all these parameter , i am getting LHR Data Ready Error.
can any one please tell what am i doing wrong.