Other Parts Discussed in Thread: MSP430F5529, , MSP430WARE, TDC7201
I am using the MSP430F5529 USB launchpad as well as the TDC7201-ZAX-EVM for a LIDAR system and was hoping to import the measurements into MATLAB to calculate the distance. I'm not totally sure of the best way to do this however. Any insight? My goal is to use Matlab to create a GUI that displays the target range and nothing else. I was also wondering if it's possible to display the range as it changes (from 20cm to 10m at the extremes). Any help that could be given would be very helpful.