This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: Programming AWR1243 with DCA1000EVM

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: DCA1000EVM, , AWR1243

I have 2 questions:

  • Do we need a DEVPACK to run RadarStudio? Can I just use the AWR1243BOOST and DCA1000EVM as a standalone for programming the chirps in the 1243?
  • Can we implement BPM coding in the Transmits using the DCA1000EVM alone?

  • Hi Rahul,

    1) DCA1000EVM can be used for device programming and to capture the adc data. Whereas DevPack can be used only for programming/configure the device.

    2) You can use mmWave Studio to configure the device (AWR1243) for required BPM codes where AWR1243 should be connected with DCA1000EVM. 

    DCA1000EVM acts as a bridge b/w AWR1243 and PC for SPI communication and LVDS transfer.

    Regards,

    Jitendra