Due to a firmware update, to our product that uses the PGA900, we have been doing some tests in the last few days. One test was sensor failure reaction. We have set the AFEDIAG_CFG register to 0x00, so there should be 4MΩ pull-down resistors on the VINPP and VINPN signals. So we would expect those signals to be close to 0V when disconnected. This is not what we measure however. When disconnected we measure ≈0,32V on VINPP. If we set AFEDIAG_CFG to 0x03 so the pull-down resistors are 1MΩ then we measure ≈0,15V on VINPP.
Do you have an idea why we do not measure 0V here?
Regards Bernd