This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC2112: Ferrite sheet

Part Number: LDC2112

Hi Kristin

If LED is placed on the surface of the LED FPC and the target metal is paste behind. ITB FPC is a coil

I refer to the specification sona957a, and put ferrite on the back of ITB FPC.

There is no hole in the target metal. Will the target inductance be reduced? Are there any risks with this design?

Thank you

URL:e2e.ti.com/.../inductive-sensing-how-to-shield-from-metal-interference

  • Hi Alex,

    This looks like a better solution than the options you previously shared with cutouts in the target metal. I have two comments:

    1. What is the gray layer in between the ITB FPC and the ferrite? In this stack-up, the metal FPC stiffener would act as the target for the sensor coil on the ITB FPC. If there is another layer of metal directly below the ITB FPC, then the sensor coil will likely not be able to detect the metal FPC stiffener. The ferrite needs to be positioned in between the sensor coil and the interfering metal in order to be effective. 

    2. The LEDs may impact the mechanical response of the button, but I've not seen this type of design before so I can't advise what kind of problems could occur. It may not cause any problems, or it may cause significant problems.

    Best Regards,

  • Hi Kristin

    1. The gray layer is a stiffener and the material is FR4. Paste the ferrite under the stiffener to prevent components interference.

    2. Thanks for your remind. The mechanical engineer will pay attention to it.

    Details of each layer.

  • Hi Kristin

    Do you have any recommendations about stack up? thanks.

  • Hi Alex,

    This stack up looks good to me.

    Best Regards,