Hi Expert,
Is the capacitance between terminals of FDC2214 reversible to temperature change?
Is the temperature change rate the same for each channel?
Thanks
Muk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
Is the capacitance between terminals of FDC2214 reversible to temperature change?
Is the temperature change rate the same for each channel?
Thanks
Muk
Temperature drift impacts:
- reference oscillator (either internal or external)
- external components (capacitors and inductors)
- capacitive sensor
If the same components are used across all channels, then they should have a similar temperature drift. So one channel could be used as a reference.