Other Parts Discussed in Thread: IWR1443BOOST, , IWR1443, IWR1843
Hi Everyone,
We are comparing IWR1843Boost and IWR1443Boost. would like to know more about IWR1843Boost as less information is available.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Everyone,
We are comparing IWR1843Boost and IWR1443Boost. would like to know more about IWR1843Boost as less information is available.
Please find my response below:
Thanks Yogesh,
That makes me comfortable to switch to IWR1843boost.
Last point .... number of objects detected per frame are max 64 in IWR1443 what about IWR1843?
Will I get same number of objects (max) per frame?
Thank you,
AA
Hi AA,
The max number of object/points that can be detected in a frame for IWR1843 is 500.
#define DPC_OBJDET_MAX_NUM_OBJECTS 500U
Thankls
Yogesh
Hello TI team and everyone else,
This is related to max detected objects/points (500) with IWR1843BOOST.
(1) Does it gives binned like data from a given object (fixed spacing between point co-ordinates along with X, Y and /or Z axis? If yes, what will be the spacing?
(2) If I restrict the angle of arrival (such that I will be to image 30 x 30 cm at close distance ), will I get all 500 points within my restricted angles?
Thanks for reply.
Regards,
Jaidip.
Hi Jaidip,
I am not able to understand the question completely. Could you please provide some context or use case to help us understand.
Thanks
Yogesh