1) We are trying to measure very small displacement (around 1mm) of a target that is quite close (1meter) to the radar. Is there possible guidelines or issues we need to consider for this?
2) When I try to find the single target using FFT magnitude, I get very different values in magnitude. How can I make it run consistent? Can the CalibDCRange setting help in this scenario? There is no other target except for a corner reflector at that 1m distance.
3) Assuming the distance bin won't change, we measure the phase difference to denote change in distance. What if the target moves to another bin, how can I make the transition in phase a bit 'smooth' and not discontinuous?
Thanks.