Hallo TI,
Currently we are using AWR1843BOOST board along with vehicle occupant detection demo for detecting a moving target. Below are few things we would like to know.
1. Currently the maximum range of this demo is 3 meters, we would like to minimize it to 1 meter. Is it possible to decrease the maximum range of the demo?
2. The current demo uses resolution of 4,7cm (3m/64 Rows). Is it possible to change the resolution to 2.3 cm(3m/128 Rows) or further more?
3. As far as I understood current demo uses only 2 Tx antennas, Is there any way I could include the Z-axis for this demo?
If any of the above mentioned are possible, Please direct me where exactly I can change in the code.
Thank you.
Best Regards,
Venkatesh Vasanthapu.