Other Parts Discussed in Thread: MMWCAS-RF-EVM
Hello
I'm connecting 4 AWR1243Ps and an external host with SPIs, and trying to control these AWR1243Ps using mmwaveLink API.
The trigger mode is "Hw triggered mode" and "SUB FRAMETRIGGER" is enable, and the external host sends a pulse to the SYUNC_IN pins of AWR1243Ps.
At that time, I noticed that the state of the WARM_RESET PINs changed from time to time.
I know that the state of WARM_RESET PIN changes when AWR1243P is powered on.
www.ti.com/.../awr1243.pdf
p.21
[Question]What are the conditions under which the state of the WARM_RESET PIN changes except when the AWR1243P is powered on?