Part Number: PGA900EVM
Tool/software: Code Composer Studio
Hello, I want to check the two-wire current loop mode, 4-20mA, I have the PGA900EVM board connected to the PGA900 GUI application with the USB2ANY, in the software I put RLOOP 10ohm. put the jumpers in current mode, and connect the jumper (J1, J2, J3) to test the 4-20mA loop, but the current loop I get is greater than 150mA.
For the PGA900 GUI software to communicate correctly with the PGA900EVM board, must the board be powered with 24V (J20-J21)? Does the PGA900 that comes with the board already have a firmware recorded? Is it ready to be used with the PGA900 GUI software?