Hi,
I'm interested in knowing if we can increase the transmit power of the antenna in AWR1843BOOST? Currently the output is pegged at 12dBm with a gain of 9dB. I want to increase the transmit power to 24dBm and gain of 9dBm (which is well under the FCC limit of 55dBm requirement). FCC re-certification is not a problem. I'm more interested in knowing if there are any other side effects (like saturation of the receive path, ability of the on board antenna to with stand this power etc).
A quick response is highly appreciated.
Thanks
Venkatesh
PS: I have seen some posts regarding the transmit power measurement and backoff but not exactly related to increasing the transmit power. Therefore a new post.