This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Reading IWR6843 LVDS raw data simultaneously from two DCA1000EVM on the same laptop.

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843

Hi,

I would like to capture the LVDS raw data of two IWR6843 simultaneously using two DCA1000EVM on the same laptop. Since the HOST PC (Ethernet cards) must be set to a static IP 192.168.33.30, so my questions are:

    - Is it possible to connect two DCA1000EVM to two Ethernet Cards on the same laptopn and capture the LVDS raw data of two sensors simultaneously ?

    - Can I simply set both of the Ethernet Cards to the same IP address 192.168.33.30? Will they work?

Thanks,

Bien