This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: Generating CW profile instead of Chirp

Part Number: TIDEP-01012
Other Parts Discussed in Thread: AWR1243BOOST

Hi,

Can you please tell if it is possible to generate CW profile instead of FMCW i.e. can we set the ramp bandwidth to zero. I am thinking of generating binary PMCW profiles using TIDEP-01012 imaging cascaded radar module.

Regards

Hamza  

  • Hi Malik, 

    Have you already tried setting up a CW TX or RX mode using the mmWave STudio lua script API? It should be very similar to the CW mode setup on the single-device AWR1243BOOST, but with the Cascade setup details setup as well. 

    I will check on this on my end as well and get back to you in a few days. 

    Thank you,

    -Randy