Part Number: TMP117
Other Parts Discussed in Thread: TMP116
Hi Team,
My customer would like to get the MSP430-Code or sample code for using TMP117. Could you please share me by email? My customer has an NDA confidential agreement. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Olin -
then add TMP117 and files will be generated for you to download and use.
Hi Josh,
Thanks for your reply. I have one other question: can this program be use for any kind of MCU such MSP430 or ST-MCU?
Thanks.
These are .c and .h files that are MCU agnostic - so yes, could be MSP430G2x, MSP430FRx, MSP430F5x, a SimpleLink MCU or other vendor.
Also, if it helps more, you see here on ti-rex: http://dev.ti.com/tirex/explore/node?node=AGd0PGb13zae3DT2fN04Cg__swcUKHN__LATEST
for example using MSP432P401R LaunchPad, there is a demo project for the TMP116. This is same as what is needed for the TMP117 and they will add soon to this officially, but the fact is you can use this example with the TMP116 or TMP117.
Ok, thanks. By the way, please take a look my other email for TMP117 question. Look forward to your reply. Thank you very much!