This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243:CSI level matching

Part Number: AWR1243


The CSI power of the processor is 1.2v, does it match the 1.8v power CSI of AWR1243?They're both d-phy.

  • Hi,

    We will need a few day to get back to you

    thank you

    Cesar

  • Hello, looking forward to your reply.

    I checked the d-phy V1.1 specification of MIPI, which stipulated that LP Transmitter VOH was 1.1v-1.3v.

    In the datasheet of AWR1243, the mode level of lp-11 is VOH. According to the datasheet specification, the minimum VOH is 1.35v under the power supply of 1.8v, which is inconsistent with the d-phy specification.

    thank you

  • Hello,

    As long as the receiver is MIPI spec compliant it should not be an issue. How they have implemented the power supply network should not matter (even though I am surprised that the D-Phy receiver is operating of only 1.2V supply).

    The VOH table you are referring to in the 1243 datasheet  are for digital IOs and not CSI signals. There is a separate CSI section where the timings are mentioned and remaining specs are based on the MIPI D-Phy specs.

    Regards,

    Vivek