This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: LMP91000

Part Number: LMP91000

Hi,

We are using LMP91000 for measurement of Blood Glucose. The current settings we are using - 

VDD = 3.3V

TIACN - TIA_GAIN = 3.5Kohm

Rload = 10ohm

REFCN = REF_SOURCE = Internal 0 

INT_Z = 50% 

BIAS = 0%

The OP_MODE is set to 3 lead amperometric mode. 

We are not seeing any voltage at WE,RE and CE electrode. 

Could you please help us to set the AFE? 

Thank you,

Seema