Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843ISK, IWR6843
Hi,
I have the following setup:
- DCA1000EVM
- MMWAVEICBOOST
- IWR6843ISK
- Two 5V 3A adapaters
Ethernet Cable not plugged in on the photo. But it was during the testing.
I am trying to use the DCA1000EVM, I have followed the Quick Start Guide and the Online training video. I keep getting the following error, where it passes everything untill it's sending its command to the DCA. This is with both following the Online Video and using the Demo Data Capture script. I have configured the Static IP Adress, Firewall is disabled, tried different ethernet cables and turned of Wifi. The IWR6843ISK works fine when using the online demo visualizer.
[14:26:36] SelectCaptureDevice Success
[14:26:36] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
[14:26:36] [RadarAPI]: Sending fpga command to DCA1000
[14:26:46] [RadarAPI]:
[14:26:46] FPGA Configuration :
[14:26:46] Timeout Error! System disconnected
[14:26:46] [RadarAPI]: Sending fpga_version command to DCA1000
[14:26:56] [RadarAPI]:
[14:26:56]
[14:26:56] Unable to read FPGA Version. [error -5]
[14:26:56]
[14:26:56] CaptureCardConfig_EthInit Success
[14:26:56] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
[14:26:56] [RadarAPI]: Sending fpga command to DCA1000
[14:27:06] [RadarAPI]:
[14:27:06] FPGA Configuration :
[14:27:06] Timeout Error! System disconnected
[14:27:06] CaptureCardConfig_Mode Success
[14:27:06] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[14:27:06] [RadarAPI]: Sending fpga command to DCA1000
[14:27:16] [RadarAPI]:
[14:27:16] FPGA Configuration :
[14:27:16] Timeout Error! System disconnected
[14:27:16] [RadarAPI]: Sending record command to DCA1000
[14:27:26] [RadarAPI]:
[14:27:26] Configure Record :
[14:27:26] Timeout Error! System disconnected
[14:27:26] CaptureCardConfig_PacketDelay failure
[14:27:26] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[14:27:26] [RadarAPI]: Sending start_record command to DCA1000
[14:27:26] [RadarAPI]: Status: Passed
[14:27:27] [RadarAPI]: ar1.StartFrame()
[14:27:27] [RadarAPI]: Status: Passed
[14:27:27] Frame start async event received!
[14:27:28] [RadarAPI]: Frame Ended
[14:27:28] Frame End async event received!
[14:27:32] Please wait for a few seconds for matlab post processing .....!!!!
[14:27:32] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[14:27:32] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
[14:27:32] Error : The number of files captured is zero!
[14:27:39]
[14:27:39] *** Script aborted by user ***
So one thing I haven't done is programming the DCA to version 2.8. I connected the DCA and tried to program it with the Diamond Programmer Tool(following the programming guide in section 9 of the DCA User's guide). This gave me the following error when clicking on the program button to erase the device.
Device#1 LFE5UM-85F: Failed to verify the ID
(Expected: 0x01113043 Read: 0xFFFFFFFF).
The setup shown below: