Hello,
In the MMWCAS-RF-EVM schematic, the control signals for the PMIC (e.g. I2C, EN, NRST, etc) are pulled up to the "PMIC1_3V3" rail. That rail is generated by a 1ohm/1.96kohm divider from the 5V supply, which makes it seem that it is actually a 5V rail. Is that correct? Is it expected that the pullups go to 5V? What are the requirements on the driver of those signals?
Thanks,
Antonio