Other Parts Discussed in Thread: TIDA-00322, TDC1000, TDC1000-C2000EVM, TUSS4470, TDC7200
I am creating a novel ultrasonic device, I will be using the TDC1011 analog front end AFE which is capable of producing 4mhz. This AFE produces the wave (pulse) and catch the echo coming back thorough the the same piezo sensor. My questions are:
1. This AFE required a clock generator. Can use any clock generator sold by IT, if yes, which one?.
2. Can the sample and data rate be adjusted on this AFE?
3. How fast my controller (in MHZ) like arduino or the IT MCU controller need to be in order to catch or read the signal coming from the AFE?.
4. what would the data transfer rate of the AFE going to the controller like a MCU or arduino?
5. How can I increase the pulse (intensity) generated by the AFE so I can have a more intense ultrasound wave from the piezo? not sure if the 3 or 5v will be enough to produce the intensity needed or maybe the desire intensity I am looking for is not needed since the echo coming back to the piezo can be amplified by the AFE?. Please any comment would be appreciated.
6. once the tdc1011 convert the signal to digital I am assuming I will get all the signal in digital form at the desired sample rate but will I also get the time of flight once the AFE stop?