Hi Team,
The customer is experiencing below issue and needs your help.
***********************************************************************************************************************************************************************************
Use "PEAK PCAN-USB Pro" do CAN-FD test , result is fail , but change to "CANFD_MCANFrameType_CLASSIC", then test result is OK.
Test environment: Windows 10
Test device: PEAK, PCAN-USB Pro (w/CAN FD)
Test tool: PCAN-View (Version 4.2.4.564)
Bit rate: 500kBits/s data rate:2Mbits/s
AWR1843 connect to PEAK PCAN-USB Pro than to PC
***********************************************************************************************************************************************************************************
Thanks.