HI Expert,
In Advanced Frame config where I have 1 sub-frame in a frame. 1 defined profile with 12 TX and 16 RX enabled in the system. There are 20 burst in a sub-frame and there are 128 chirps in the burst configured to chirp out of all 12 TX channels. I also want to loop over 64 times. My questions below:
1. How are 128 chirps being transmitted out of the 12 TX channels? My understanding is that all 12 TX channels transmit the 128 chirps simultaneously 12 at a time until the 128 chirps in the burst is exhausted before moving on to the next burst in the sub-frame.
2. What is my number of virtual channels in this case?
3. What is my radar cube look like?
4. How can I map this configuration to Processor SDK?
5. Would normal frame config even work for this case if I don't want to use Advanced Frame Config?
Thanks,
--Khai