Other Parts Discussed in Thread: MMWCAS-DSP-EVM
Hi,
I am trying to change the chirp setting and measure using "Cascade_Configuration_MIMO.lua"
In the attached file condition, "ADC Samples" was confirmed to work properly under the conditions of 256 and 512, but when it was 1024, measurement failed due to a timeout error.
Could you tell me the cause and how to measure at 1024 points?
#When "Cascade_Capture.lua" is executed, an error occurs even though "Cascade_Configuration_MIMO.lua" is completed normally.
#The details of the error are as follows.
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
[13:21:36] Loops Remaining : 1
[13:21:36] Starting TDA ARM...
[13:21:36] [RadarAPI]: ar1.TDACaptureCard_StartRecord_mult(1, 0, 0, Cas_Cap_200316, 0)
[13:21:36] Device 0 - Configuring TDA with Width : 8192 and Height : 192
[13:21:36] [RadarAPI]: Device 0 - setWidthAndHeight Status: Passed
[13:21:36] Device 1 - Configuring TDA with Width : 8192 and Height : 192
[13:21:36] [RadarAPI]: Device 1 - setWidthAndHeight Status: Passed
[13:21:36] Device 2 - Configuring TDA with Width : 8192 and Height : 192
[13:21:36] [RadarAPI]: Device 2 - setWidthAndHeight Status: Passed
[13:21:36] Device 3 - Configuring TDA with Width : 8192 and Height : 192
[13:21:36] [RadarAPI]: Device 3 - setWidthAndHeight Status: Passed
[13:21:36] Sending Frame Periodicity of 100 to TDA..
[13:21:36] [RadarAPI]: Status: Passed. Frame Periodicity sent to TDA
[13:21:39] Frame Periodicity Response from Capture Card timed out!!
[13:21:39] TDA ARM Failed