Hi,
1. The amplitude of illumXtalk calibration is close to 15,000, and the register force_scale_val needs to be set to 5 to complete the calibration.Why is the bottom noise so high?
2. During the measurement process, the target object increases in amplitude from far to near, but when it reaches more than 10,000, it jumps directly to 65536 with a distance of 0 and cannot be measured.Why will the strength appear fault phenomenon, how to solve?
Thanks!