This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: 1D/2D FFT source code, Doppler bins

Part Number: AWR1243

Hi,

1.According to the manual, 1D/2D FFT is made on EVE core. Can I see the source code(MIMO & TxBF)? I didn't find them in the SDK.

2.There was an error when I changed the doppler model from 64 to 128 (MIMO mode) :

The explanation I saw in another post:

But this error still exists after I changed the frame cycle from 100ms to 200ms.

And if I increase the number of samples from 256 to 512, I get the same error.

This is the configuration I'm using now:

Which parameter should I change to eliminate this error?

Regards,

JG